More energy-efficient pump station
UK
Challenge Four high-efficiency 100 kW Flygt N-pumps operating with variable frequency drives (VFDs) deliver a total volume of 0.8 m3/s (12,700 US gpm) and consume 1,000,000 kWh of energy per year....
• 卓越的无堵塞性能
• 自清洁无堵塞叶轮
• 多叶片设计,在废水中可实现最高效率
• 持续高效
• 硬铸铁,可选双相不锈钢和硬铁叶轮
Whether you would like additional information or are interested in getting a quote, we're here to help.
All fields required.
用于严苛废水泵送的显而易见的选择
Flygt的自清洁非阻塞N泵具有创新的设计和功能,可提供持续高效率和最可靠的运行。从而使得该类泵成为广泛严苛废水应用情形的最可靠选择,例如:未安置滤网的污水、废水以及固体浓度高达8%的污泥。Flygt N泵的最大处理能力可达1000 l/s(16.000 gpm),电动机功率从1.3至680 kW(1.5至870 hp)、水头可达100 m(330 ft)。
选择硬铸铁叶轮用于典型的废水应用情形,或选择切碎叶轮用于具有长纤维和重固体的最严苛应用情形。对于带有沙子、砂砾和其他磨蚀性物质的所有应用情形以及混合海水的废水,强度推荐使用Hard-Iron™叶轮。对于特殊应用(例如高度腐蚀性废水环境),我们提供双相不锈钢叶轮。
UK
Challenge Four high-efficiency 100 kW Flygt N-pumps operating with variable frequency drives (VFDs) deliver a total volume of 0.8 m3/s (12,700 US gpm) and consume 1,000,000 kWh of energy per year....
UK
Challenge At one of the largest wastewater treatment plants in the Midlands, a strategic pump station was at risk of complete failure and required fast and efficient replacement within the shortest...
SWEDEN
To prevent pollution by sewage from ships, governments are required to ensure the provision of adequate sewage reception facilities. One of the ports within the Ports of Stockholm were outfitted with...
USA
Jefferson Parish sewer rates are among the lowest in the country for a system of this size and economic importance to the region. Even routine storms can spawn enough rainfall to induce surges of...
UK
England’s Northumbrian Water Ltd (NWL) serves roughly 2.5 million people with water and sewerage services. To better assess its predicted results they conducted a project to measure how much the...
NEW ZEALAND
Frequent blockages and the challenges associated with high temperature geothermal environments put extreme demands on this pumping station. A lot of different solutions had been suggested before the...
Water and Sanitation, City of Montmorillon
Montmorillon, France
A cleaner sump requiring fewer drainage operations thanks to Xylem’s sustainable wastewater pumping solution Xylem’s revolutionary Flygt Experior wastewater pumping system has reduced the annual...
ITALY
Challenge The region's heavy dependence on tourism puts a strong focus on maintaining the quality of the local environment. A complex pump station management system oversees a total of 14 pumping...
ITALY
One of Sardinia’s largest water treatment facilities needed an energy efficient and sustainable pumping solution. Flygt Experior was installed giving exactly that, reducing the energy consumption by...
UNITED KINGDOM
Challenge Heathrow Airport Water Services Department commissioned Xylem to evaluate the wastewater pumping system in the cargo center area of the airport which hosts heavy volumes of traffic and...
SWEDEN
Built in 2006, the Sigtuna pump station has two Flygt N 3153 HT pumps, originally started via soft starters. In 2011, Xylem installed Flygt SmartRun pump controller on each pump in the Sigtuna...
SWEDEN
Challenge During the spring, when the snow is melting, as well as with heavy rainfall, the inflow to the station increases dramatically. To prevent the station from flooding, the pumps must be sized...