It looks like you are coming from United States, but the current site you have selected to visit is Croatia. Do you want to change site?

Yes, please! No, keep me on the current site

Pump station retrofit ends stormwater woes in Lyndhurst, NJ

A Bergen County, New Jersey, riverside town receives relief from torturous flooding after its stormwater pumping station is dramatically improved by the installation of new Flygt pumps

Challenge

Failing, old, long shaft pumps at the Lyndhurst Sewer Department’s stormwater station were out on maintenance issues more than in operation. Existing pumping equipment was noisy, prone to blockage by debris, and suffered from lube system problems. Removing the equipment for service was not only a challenge, it was also expensive.

Solution

Pump replacement included a strong preference for a submersible-pump solution by Lyndhurst officials. Lyndhurst DPW was already very familiar with Flygt’s reliability and the services provided by Pumping Services, Inc., the pump manufacturer’s local representative. After careful review of the pump’s axial flow design, it was decided to go with mixed flow units. The mixed flow pump units offer a compact footprint that could be efficiently incorporated into the existing station clear well. In addition, the axial flow pump can operate in a less than ideal wet well layout and are able to handle difficult flood water debris, such as branches, leaves, weeds, trash, and sediments like sand, silt, mud, and soil.