It looks like you are coming from United States, but the current site you have selected to visit is Canada. Do you want to change sites?

Yes, please. No. Keep me on the current site.

4-20 mA Controlled Pumps

Many transmitters and other water treatment equipment can provide a 4-20mA analog signal that can be used to control output of a metering pump. Pulsatron E Plus Series feeders have optional 4-20mA input control along with manual controls (100:1 turndown ratio). Fully scalable 4-20mA input controls are standard on the microprocessor controlled Pulsatron MP Series feeders which also have more precise 1000:1 turndown ratio manual controls.

4-20 mA Controlled Pumps