It looks like you are coming from United States, but the current site you have selected to visit is Australia. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Enable high contrast mode

Reverse Osmosis (RO) Systems / Nanofiltration Systems

Reverse osmosis (RO) and Nanofiltration (NF) membranes are commonly used as a filtration method to remove many types of dissolved solids (large molecules and ions) from solutions by applying pressure to the solution when it is on one side of a selective membrane. The result is that the solute is retained on the pressurized side of the membrane and the pure solvent is allowed to pass to the other side.

Reverse Osmosis (RO) Systems / Nanofiltration Systems

  • Vantage® M41RS (Select)

    Vantage® M41 RS Reverse Osmosis (RO) units are pre-engineered and pre-assembled units designed for a variety of industrial and commercial applications. RO...
  • Vantage® M43 Reverse Osmosis Systems

    Vantage® M43 Reverse Osmosis (RO) units are pre-engineered and pre-assembled units designed for a variety of industrial and commercial applications. RO...
  • Vantage® M83 Reverse Osmosis Systems

    Vantage® M83 Reverse Osmosis (RO) units are pre-engineered and pre-assembled units designed for a variety of industrial and commercial applications. RO...
  • Vantage® M84 Reverse Osmosis Systems

    Vantage® M84 Reverse Osmosis (RO) units are pre-engineered and pre-assembled units designed for a variety of industrial and commercial applications. RO...
  • Vantage® M86 Reverse Osmosis Systems

    Vantage ® M86 Reverse Osmosis (RO) units are pre-engineered and pre-assembled units designed for a variety of industrial and commercial applications. RO...
  • Vantage® M284 Reverse Osmosis Systems

    Vantage® M284 Reverse Osmosis (RO) units are pre-engineered and pre-assembled units designed for a variety of industrial and commercial applications. RO...
  • Vantage® M286 Reverse Osmosis Systems

    Vantage® M286 Reverse Osmosis (RO) units are pre-engineered and pre-assembled units designed for a variety of industrial and commercial applications. RO...
  • 23G Central RO System

    Hemodialysis providers and patients around the world rely on the 23G reverse osmosis system for push button simplicity and reliability. This service friendly...
  • 700 Reverse Osmosis System

    With five different models to choose from, the 700 Series dialysis reverse osmosis system provides increased water production capacity, standard monitoring...
  • BioPure HX2 Dialysis Water System

    Mar Cor Purification offers the next generation central RO unit, the BioPure HX2. This direct feed double pass reverse osmosis system is designed specially to...
  • CIP Tank

    Clean in Place Tank for Portable RO Systems Designed for Clean-In-Place applications, This tank features a light weight, stable construction and spill proof...
  • CWP Dialysis Water System

    The CWP 100 offers cost-effective, consistent delivery of AAMI grade water, according to ANSI/AAMI 13959 for dialysis at the point of use. This system is...
  • ENX Filter

    Ultrafilter for Endotoxin Removal Filter for Use in Hemodialysis Water and Concentrate Devices. The ENX Endotoxin Ultrafilter assists in preparing water or...
  • Tx3 Therapy Supply Station

    Cleaner. More Durable. Discover an Innovation in Dialysis Wall Box Stations A reimagined dialysis workstation that’s clean and durable. As connection...
  • MCB Series Bicarbonate System

    50-100 Gallon Tanks, Mix & Delivery Our Bicarb Mixing and Distribution Systems are cost-effective, clean and effcient, and are the best designs in the...
  • Millenium HX Dialysis Water System

    Isolated Automated Heat Disinfection The Millenium HX water purification system is a break-through portable RO unit. This compact RO represents a quantum leap...
  • Minncare HD Disinfection Kit

    Easily Disinfect Your Portable Water System Minncare® HD is the first chemical disinfectant to hold a FDA 510(k) cleared claim for the disinfection of water...
  • PTG-520 Carbon Block System

    The Carbon Block Filtration System is a filtration device designed to remove chlorine and/or chloramines for an incoming water supply. This pretreatment unit...
  • PTS-47 Pretreatment Testing Station

    The PTS-47 is a Pretreatment Testing Station specifically designed for hemodialysis water treatment systems. It serves as a collection site for the express...
  • Rover ALX Dialysis Water Transport System

    Compact All-In-One Water Treatment Delivery System The ROVER ALX dialysis water transport system is our smallest transport system footprint designed to fit the...
  • SDS and PSDS Bicarbonate Systems

    Our Bicarb Mixing and Distribution Systems are cost-eective, clean and ecient, and are industry leading systems. We oer a range of choices so you can...

Create Wishlist

Add to wishlists
Select one or more wishlists.

Item successfully added to wishlist.

Item successfully added to new wishlist.
Item successfully added to existing wishlist.