It looks like you are coming from United States, but the current site you have selected to visit is Europe. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

On-Site Hypochlorite Generation Systems

OSEC systems safely generate sodium hypochlorite on-demand, using only salt, water and power. With over 30 years of history installing OSHG systems throughout the world, our branded OSEC system is suited to many applications across municipal, aquatics and industrial markets.

Benefits Include:

  • Sodium hypochlorite is generated through a highly efficient in-situ process allowing economic production according to the actual demand.
  • Hypochlorite product is generated on-site and on-demand from inert feedstocks, reducing or eliminating common issues with chemical storage and handling.
  • Low strength solution at a stable concentration means minimized decomposition of active chlorine in solution always available.
  • Product generated with minimized disinfection by-product formation and further cost savings can be achieved via off-peak production scheduling.

On-Site Hypochlorite Generation Systems

Create Wishlist

Add to wishlists
Select one or more wishlists.

Item successfully added to wishlist.

Item successfully added to new wishlist.
Item successfully added to existing wishlist.