It looks like you are coming from United States, but the current site you have selected to visit is Turkey. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Flygt Pumps in the Alicante II Desalination Plant (Spain)

Background

Seawater Desalination Case Study Image 1.pngAlicante is the centre of one of the largest tourist areas in Spain in the middle of the Mediterranean coast, and gets 80% of its drinking water from desalination plants.

Desalination ensures a sufficient supply of water to meet the expected growing demand of over 2 million people, which increases to 3 million in the summer season.

There are 2 plants in the south of Alicante, each with an annual capacity of 24 hm3. Alicante II is the most modern and is located along the coastal strip between Agua Amarga and El Altet beach, near the other seawater desalination facility, Alicante I, in operation since the end of 2003.

“80% of the drinking water consumed is obtained from desalination plants.”

Collection and pumping of seawater

Seawater Desalination Case Study Image 2.pngThere are basically two ways of capturing sea water for desalination: open catchment or with wells. Wells produce a better quality of incoming water, because the land acts as a filter, and they have less environmental impact.

In the initial project, this tank was divided into two zones: one for water and the other for dry installed pumps, separated by a wall. There were 7 + 1 pumps, each with a flow of 915 m3 per hour @ 85 mca, controlled by frequency converters.

When Xylem was consulted about this solution, submerged pumps were given as an alternative.

The main arguments presented by Xylem Iberia for this were as follows:

  • Digging was reduced with submerged pumps as the room to install the dry pumps, the interconnecting pipes, the stairs and access were completely eliminated.
  • The wall dividing the water chamber from the pumping chamber is very expensive, because it needs to withstand the entire water pressure on just one side.

This solution was accepted after some discussion and the selection process for submersible pumps was started. This time, other companies in addition to Xylem were consulted, which offered different types of submersible pumps, some of them with special stainless steel, such as duplex or Superduplex. Xylem offered conventional pumps (CP), with zinc anodes, epoxy paint and galvanic protection.

“Xylem has a lot of experience using adequately protected Flygt pumps in seawater with excellent results.”
  • Xylem has a lot of experience and excellent results using Flygt pumps which are adequately protected (with zinc anodes and especially epoxy paint) in seawater, in both municipal and industrial applications, such as aquaculture.
  • The use of conventional pumps widens the selection options, as they can be adapted to the specific operation of the plant while optimising efficiency in the facility.
  • Using special alloys increases the price of the pumps by 3-5 times, with no other advantages apart from lower maintenance, as the anodes do not need to be replaced. 
  • To increase the useful life of the anodes, Xylem uses impressed current cathodic protection (ICCP), a system widely used in industrial applications, such as shipyards and buried pipelines. 
  • The delivery period for pumps in duplexes is much greater than that of conventional pumps. This is not only important for the first delivery, but also for each time a replacement part is needed throughout the life of the pump.
  • If a duplex pump fails, only some workshops are able to repair them and they will probably lack spare parts.

In the same tank, another 2 Flygt submersible pumps (1 +1) of 72 m3/h at 20 mca were installed to empty the tank if necessary.

Seawater Desalination Case Study Image 3.pngAll pumps in this tank are protected by current cathodic protection, zinc anodes and epoxy paint.

In this project, Xylem Iberia also supplied 4 Flygt axial flow pumps, model PL 7101/865 230 kW, working at 595 rpm, protected by epoxy paint and zinc anodes, to pump seawater for the dilution of the brine from the two desalination plants (Alicante I and II) before being discharged into the sea (6 parts of seawater to 1 part brine).

The brine from both desalination plants is pumped with 3 x 90 kW Flygt pumps, model PL 7101/805, (2 of which were supplied for the Alicante I plant in 2005), all protected with epoxy paint and zinc anodes.

Finally, Xylem supplied the pumping for treated water, consisting of 3 split-bed pumps (2 + 1) of 1440 m3/h at 110 mca controlled with a frequency variator and the cartridges that protect the reverse osmosis membranes.

Current situation

The Alicante II plant started operation in July 2008. Since then, Xylem Iberia has supervised the operation and maintenance of submersible pumps.

During this period, the current cathodic protection has worked very well by increasing the life of the zinc anodes and protecting the pumps, which have suffered no corrosion problems.

Seawater Desalination Case Study Image 4.pngAfter more than a year of operation, in October 2009, a team of divers took out 2 pumps from the lower part of the tank for a complete inspection and to verify the proper condition of the pump sockets. For safety reasons, the zinc anodes are replaced every 5 months; those with the ICCP system installed are in a better state than those without this system.

Xylem is continuing research on current cathodic protection to extend the useful life of zinc anodes to at least 1 year, by adjusting the current in the system.