It looks like you are coming from United States, but the current site you have selected to visit is Thailand. Do you want to change site?

Yes, please! No, keep me on the current site

Compact stormwater pump station

USA

Challenge

Placement of a new stormwater pump station in a 10 m x 5 m (32 × 18 ft) area between two roads and a hotel in one mid-western state’s major cities. Close proximity to three rivers, snow melting during the springtime and heavy rainfall during the summer posed flooding risks to the area.

Solution
A compact stormwater station with excellent hydraulics within the limited space using Flygt propeller pumps and Flygt Formed Suction Intake devices. Each pump is rated 280 HP and designed to pump 2 m3/s (31,600 US gpm) at 7 m (22 ft) TDH. Thanks to the use of the Flygt FSI devices, the station was able to handle 22 cm (9 in.) of rainfall in a single day. The station is so compact that it can accommodate an additional pump should expansion be necessary in the future.