-
EnviroMix BioCycle-D helps WWTP meet stringent limits in Boxelder, CO
See how Boxelder Sanitation District upgraded its Fort Collins-area WWTP to meet stricter nitrogen and phosphorus limits with EnviroMix BioCycle-D optimized aerobic digestion. The decoupled aeration and mixing approach cut projected energy use by 75% versus conventional estimates and is saving more than $175,000 annually. -
EnviroMix BioMix delivers completely mixed anoxic zones in Ventura, CA
See how Ventura’s Water Reclamation Facility solved sludge settling and septic corners in its BNR anoxic zones by replacing ten submersible mixers with EnviroMix BioMix compressed gas mixing. The result was complete mixing with negligible oxygen transfer and estimated energy and maintenance savings of more than $60,000 per year. -
EnviroMix BioMix provides O&M savings in Russellville, AR
See how Russellville’s Pollution Control Works reduced operating costs with BioMix compressed gas mixing and achieved 75% energy savings in Phase I and more than 60% in Phase II versus mechanical mixers. -
EnviroMix BioCycle-D delivers AL plant low-maintenance aerobic digestion
Read how the Eastside Wastewater Treatment Plant in Albertville, AL used the EnviroMix BioCycle-D™ process to simplify operations, reduce maintenance, and improve energy efficiency. -
Realtime monitoring cuts pollution risk at Scottish Water site
When a critical pumping station failed, Scottish Water used Xylem Vue Secure Connect monitoring and real-time data to restore resilience and protect the environment. -
Beating the blockages at Rochfort Manor
How Flygt Concertor eliminated pump blockages, improved reliability, and delivered over 70% energy savings for Irish Water. -
Zero unplanned failures since 2013
Planned Maintenance Agreement delivers budget predictability and zero unplanned failures for Municipality of Scott -
ESAMUR: comprehensive digitalization platform for advanced monitoring of the wastewater treatment system in Murcia
The REGEN-IA project, built on the Xylem Vue platform, aims to integrate, govern, and leverage ESAMUR’s operational information within a single environment. -
A clear path forward for City of Kamloops’ most critical feeder main
The City of Kamloops used Xylem's PipeDiver to inspect an aging main, gaining defensible data to extend asset life, plan a repair and refine capital priorities. -
Mimizan: reducing inflow and infiltration through centralized data collection and analysis
The Mimizan Federation of Municipalities is implementing the Xylem Vue platform to reduce inflow and infiltration by improving infrastructure monitoring. -
Redland city council: Cleveland WWTP operational improvement & data management project with Xylem Vue platform
Redland City Council unified plant operations data with Xylem Vue, boosting compliance monitoring and efficiency at Cleveland WWTP. -
Mission-critical support: Xylem powers sewage reliability aboard the USS Hornet
To help address the USS Hornet’s urgent wastewater system needs, a Xylem Goulds Water Technology 1GD51G4AA model grinder pump was recommended to replace the damaged unit that serves one of the ship’s critical onboard sewage tanks. This support provided the museum with a reliable, high-quality replacement that restored confidence in an essential system while easing the financial burden on the nonprofit organization. -
Severn Trent Water: digital twin to optimise energy and emissions in WWTPs
The implementation of a digital twin at the Strongford treatment works has enabled Severn Trent Water to visualise plant performance in near-real time. -
Pumping system with integrated intelligence eliminates chronic clogging and debris buildup in pump station
The city of Sublimity reduced maintenance costs for a problematic wastewater pump station while creating flow capacity for future residential growth. -
EMALCSA: implementation of a digital twin to support decision-making in water supply network operations
The Empresa Municipal de Aguas de La Coruña (EMALCSA) manages the water cycle in the city of A Coruña and seven neighboring municipalities, serving a total population of 400,000. The utility collects, treats and distributes over 36 million cubic meters of drinking water to 138,000 customers each year, via a network of over 560 kilometers, 26 storage tanks and six pumping stations. -
Temporary DAF system supports refinery outage
A temporary wastewater treatment system was deployed during a planned outage to support operations while two existing DAF units underwent repair. -
No margin for downtime: Redundant cooling water treatment for a hyperscale data center
A major hyperscale operator launched a new data center campus in Virginia with a clear mandate: design cooling infrastructure to prevent downtime. With high availability requirements and strict discharge constraints, the project team needed a water treatment partner that could deliver quickly, adapt to design changes midstream, and build redundancy into every critical component. -
High performance data center reduces cooling risk with phased water treatment strategy
A global leader in data center infrastructure set out to build a large-scale, high-performance computing campus in South Central U.S. Built for extreme performance— with redundant electrical topologies, full UPS and battery backup, and very high rack densities —the facility required an equally resilient water filtration system to support primary chilled water and adiabatic chiller cooling. With multi‑gigawatt‑scale power capacity, every system had to be engineered around a single imperative: continuous operation. -
ALJARAFESA: Advanced water cycle asset and work order management
Discover how ALJARAFESA modernized water cycle operations with a unified digital platform that connects asset management, maintenance, and leak detection to improve efficiency, responsiveness, and service delivery. -
Orekan (Navarre Regional Government): early warning system to reduce flood risk
The Autonomous Region of Navarre, located in northern Spain, has a surface area of over 10,000 km² and a population of approximately 680,000, concentrated mainly in the Pamplona metropolitan area. It has a highly complex hydrological system, as it is divided between the Ebro River basin, which covers approximately 90% of the region, and the Cantabrian basin, characterized by short, fast-responding basins. -
Secure in-field firmware updates to support more resilient connected products
EU Cyber Resilience Act: Manufacturers must report vulnerabilities from Sept 2026, with full compliance required by Dec 2027 -
CABB: optimization of the primary wastewater network
The Bilbao Bizkaia Water Consortium (CABB) is the public utility responsible for managing the main drinking water and wastewater network in the province of Bizkaia, serving over one million residents through a range of water supply pipelines, sewer networks, and wastewater treatment plants across 97 municipalities. -
EMASESA: implementation of a digital twin to optimize decision-making in drinking water and wastewater management
Implementation of the Xylem Vue platform to optimize management, anticipate events, and improve the efficiency, resilience, and sustainability of the water cycle in Seville. -
Faster draft beer service with Flojet pumps | Bottoms Up System
For GrinOn Industries, creators of the innovative Bottoms Up draft beer dispenser, the goal has always been simple: deliver great beer to people faster, with less waste and zero compromise on quality.