SharePoint

Products

Leveraging the experience of more than 250,000 systems installed worldwide, Xylem’s Wedeco brand manufactures reliable, chemical-free, and environmentally-friendly water and wastewater treatment technologies, including ultraviolet (UV) disinfection and ozone oxidation systems. Wedeco systems accommodate customer needs according to their individual requirements, whether it’s eliminating microorganisms in wastewater, disinfecting public drinking water, or treating process water for industrial purposes.

Wedeco Product Categories

Related Categories

Ozone Systems

For drinking water, wastewater treatment and other industrial processes.

Industries & Applications

Xylem offers a range of advanced wastewater and water solutions to help operators around the world achieve their required water effluent while delivering optimal performance, reliable operations and substantial energy savings no matter what industry or application. Working with customers, Xylem listens, learns, and adapts to local environments, ensuring the best possible design, customized to meet their specific needs. Below are some recommended industries and applications.

Wedeco UV systems offer customers an alternative to environmentally-harmful chemicals used for disinfection including chlorine, chlorine dioxide, and hypochlorite. UV disinfection is adapted from the natural action of sunlight and is extremely versatile. UV light can be used for disinfecting water, destroying harmful microorganisms in other liquids, on surfaces, and in the air. Wedeco UV systems are suited for the disinfection of drinking water, process water, wastewater, salt water, ultrapure water, and other translucent fluids, such as sugar syrup.

Ozone is one of the strongest industrially producible oxidizing agents, and is commonly used for the treatment of water in municipal and industrial applications. The special advantage of ozone is the environmentally-friendly way in which it works. Harmful substances, colors, odors, and microorganisms are destroyed directly by oxidation, without the formation of harmful, chlorinated by-products. Apart from the treatment of drinking water and wastewater, Xylem’s Wedeco ozone systems are used in bleaching processes, such as paper bleaching, as well as in other industrial oxidation processes. 

Xylem’s Wedeco brand also offers Advanced Oxidation Process (AOP) solutions that are intended to eliminate a wide variety of toxic compounds and microscopic pollutants. Xylem’s Wedeco pre-engineered AOP systems are based on three key components – ozone, hydrogen peroxide, and UV light generated by low-pressure, high-intensity lamp technology. By combining these technologies, Xylem is able to meet customer’s individual requirements.

Flygt Innovation Timeline

    1970 2000

    Contact

    Xylem has offices in 150 countries around the world. If you are looking for a location different from the ones listed below, click on "find a location" at the bottom of the page.