SharePoint

Products

Xylem’s Sanitaire brand provides complete biological wastewater treatment solutions for public utility and industrial applications. The Sanitaire comprehensive offering includes diffused aeration, sequencing batch reactors, oxidation ditches and state-of-the-art controls that drive efficient operations. Sanitaire is regarded as a leading brand in diffused aeration, which is a process that introduces air into a liquid, providing an aerobic environment for degradation of organic matter. Fine-pore diffusion of air is highly competitive due to its high oxygen transfer efficiency and lower energy costs. Sanitaire wide-band aeration systems are used in applications such as grit chambers and sludge that require non-clogging, maintenance-free systems. In 2013, Xylem launched the Sanitaire OSCAR process performance optimization system. When combined with Sanitaire advanced aeration systems, Xylem was able to deliver 65 percent energy savings to the operators of the Sterno, Sweden wastewater treatment plant.

Sanitaire Product Categories

Related Categories

Blowers

A diverse portfolio of technologies to suit any aeration need.

Jet Aerators

Stand-alone aeration system for reliable and affordable oxygen transfer.

Oxidation Ditch

Utilizes long solids retention times to remove biodegradable organics.

SCADA

Integrates process control for the entire plant.

Industries & Applications

Xylem offers a range of advanced wastewater and water solutions to help operators around the world achieve their required water effluent while delivering optimal performance, reliable operations and substantial energy savings no matter what industry or application. Working with customers, Xylem listens, learns, and adapts to local environments, ensuring the best possible design, customized to meet their specific needs. Below are some recommended industries and applications.

Established in 1967, Xylem’s Sanitaire brand provides biological wastewater treatment solutions for municipal and industrial applications. Sanitaire delivers a comprehensive offering that includes diffused aeration, oxidation ditches, membrane bioreactors (MBR), sequencing batch reactors (SBR), drum filters, and state-of-the-art controls that drive efficient operations. 

Sanitaire is regarded as a leading brand in diffused aeration, which is a process that introduces air into a liquid, providing an aerobic environment for degradation of organic matter. The broad selection of diffusers available including membrane, ceramic and coarse bubble, has been proven over time with over 22 million units installed worldwide. Xylem’s extensive applications expertise is available to ensure that both the right product is selected and the design is optimized for long-term reliability and low cost of ownership. 

Sanitaire wide-band aeration systems are used in applications such as grit chambers and sludge that require non-clogging, maintenance-free systems.

Combining Sanitaire diffused aeration, Flygt submersible mixing and overall process application, as well as instrumentation and process control in both new and retrofit applications, Xylem’s Sanitaire Bioloop oxidation ditch delivers up to 50% better energy efficiency, while remaining adaptable to a wide range of flow and loading conditions. 

Xylem’s Sanitaire MBR process combines Sanitaire diffused aeration, Flygt submersible mixing and pumps, WTW and MJK instrumentation, and unique process knowledge with Tier 1 membrane products available in the market. The result of this flexible biological design, and the complete removal of suspended solids from the treated water by ultrafiltration membranes, is superior effluent quality to meet discharge requirements. 

The Sanitaire ICEAS Advanced SBR is a continuous flow biological treatment system that provides multiple advantages versus conventional activated sludge and other SBRs by bringing together process, aeration, decanting, and control in a single treatment tank. Fully automated, it includes a completely integrated process design consisting of the aeration system, blowers, pumps, mixers, effluent decanters, monitoring and control equipment, and a comprehensive process control system.

The Sanitaire OSCAR process performance optimizer provides real-time wastewater process measurement and control to optimize operations. Combining the monitoring capability of the most advanced probes and control systems for aeration and Solids Retention Time (SRT), OSCAR reduces energy consumption while stabilizing the treatment process and maintaining effluent quality. 

Flygt Innovation Timeline

    1970 2000

    Contact

    Xylem has offices in 150 countries around the world. If you are looking for a location different from the ones listed below, click on "find a location" at the bottom of the page.